AXIS#.DEC
Description
AXIS#.DEC sets the deceleration value for the velocity loop command (AXIS#.VL.CMDU ) and for the analog
velocity command. The operation mode (AXIS#.OPMODE ) must be set to velocity mode for this command to function.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2 Linear: counts/s2, mm/s2, µm/s2 , (custom units)/s2 See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Units for details. |
|
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.DEC | 0x5000 | 0x3 | DINT | - | Acceleration | RW | False |
| AXIS2.DEC | 0x5100 | 0x3 | DINT | - | Acceleration | RW | False |
|
Copyright © 2018 Kollmorgen |
|